This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
does anyone have a precise description how to flash the DSP via CANBUS? How to set up the DSP's bootloader, how to get my program into the right format and with which software do I have to send the data to the bus?
I have a USB-to-CAN-Interface from IXXAT if this does matter.
Greetings from Germany,
Jens
Hi Jens,
you could try http://www.port.de/deutsch/canprod/sw_bootloader.html
Free binary available!
RH
Guess (as the desription is in German), this site provides a bootloader for CAN port. You still need to use/download flash API to target DSC. The following TI app note has additional info/code;
SPRAAQ2 - TMS320F281x Boot ROM Serial Flash Programming
Pradeep