This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The current updates configuration file on the controlSUITE update server location contains an error that should be fixed to retrieve updates.
The URL in the v3.2.3 section contains an “erroneous new line character” resulting in a blank URL.
In the file updates.aiu the following should be changed:
[controlSUITE_v3p2p3]
Name = controlSUITE v3.2.3 Updater
URL =
http://software-dl.ti.com/C2000/c2000_apps_public_sw/updates/controlsuiteupdater_v3.2.3.msi
Size = 71463424
Description = controlSUITE GUI Updates, New PinMux Utility, and more!
Feature1 = controlSUITE GUI Updates
Feature2 = Pin Mux Utility v102
RegistryKey = HKLM\Software\Texas Instruments, Inc.\ControlSUITE\Version
Version = >= 3.2.3
Depends = controlSUITE_v3p2p2
to get it working again in:
[controlSUITE_v3p2p3]
Name = controlSUITE v3.2.3 Updater
URL = http://software-dl.ti.com/C2000/c2000_apps_public_sw/updates/controlsuiteupdater_v3.2.3.msi
Size = 71463424
Description = controlSUITE GUI Updates, New PinMux Utility, and more!
Feature1 = controlSUITE GUI Updates
Feature2 = Pin Mux Utility v102
RegistryKey = HKLM\Software\Texas Instruments, Inc.\ControlSUITE\Version
Version = >= 3.2.3
Depends = controlSUITE_v3p2p2
See attached corrected updates.aiu file as well.
Kind regards,
Robert Beekmans
Contronics Engineering B.V.
The Netherlands
Hi Robert,
I have just installed ControlSuite 3.2.9 and have the same failure to update problem. However I don't seem to be able to find the updates.aiu file you refer to.
Dave
David Atkinson59 said:Yes, that's worked. Thanks very much for you help.
That's Great, Dave! Please close the thread.
Regards,
Gautam
Hi Gautam,
I have just joined the community and as yet I don't know how to close the thread. I can't see an obvious button for this. In the general notes on using E2E I see reference to a green "verify" button but I can't see it on the page which shows the posting and your response. I'm not even sure if hitting the "verify" button is the same as closing the thread. My original message was actually a reply to and existing thread on the controlsuite update issue so I'm not sure if I can close the thread. Can you clarify this for me and if I can close it I will do so promptly.
Cheers
Dave
Actually, you're not the thread owner and hence you can't close the thread! Please open a new thread from next time onwards as that would be easier for other users to track the posts.
Goodluck & Regards,
Gautam