This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In regard to schematic of SRAM (IS61LV6416/L) connection to F28335 for ezDSP F28335, I concern the way the address from F28335 connects to SRAM
XA0 to XA8 connect to A0 to A8 which is fine
XA9 connect to A11
XA10 connect to A12
........
XA16 connect to A9
Is there reason for doing that?
Should I implement linear address from XA0 to XA16 to A0 to A16
Hi Ric,
richard payne said:Is there reason for doing that?
No reason as such. I'm not sure why they grounded A10 in the above ezdsp board!
richard payne said:Should I implement linear address from XA0 to XA16 to A0 to A16
Yes, that should not be an issue as the device (SRAM) datasheet clearly specifies them as address lines.
Regards,
Gautam