Hello Team,
I am working on motor control application using F28069F microcontroller processor. The program is customized for F28069F microcontroller.
Due to some hardware issues, I have to use the F28069M microcontroller processor instead of F28069F microcontroller.
Is it possible to tell what all files has to be changed in the program, for using it in F28069M ?
Note : Motor control program is built using Motorware 7.
I added the linker file of the F28069M, but still no luck.
Requesting to please help me with this.
I have added the word doc, which shows screen of the Project Explorer of program,
Thanks and best regards,
Chetan.