Part Number: SM320F28335-EP
Hi,
I'm working with the F28335 EP micro.
I work with linker file that save and run the code in flash memory.
Now I'm trying to use the sprintf function but when the micro execute it the system generate and exception and finish to work.
I search on internet and I see that is a common problem. I follow also some threads on the forum as (link ) but it do not help me.
I changed in the linker the stack to 0x800 and the heap size to 0x800 but it still do not work.
I noted that if I write the in this way "sprintf(buff, "Test");" it works. But if I write the function in this way "sprintf(buff, "Test %d", var);" it fails and generate an exception.
I try with all the suggestion that I found on the forum but I did not able to use the sprintf in my project.
Thank you very much for your help.
Regards,
Andrea