Part Number: TMS320F28377D
HI ,
I have an issue with my board booting from flash.
I have developed my application code on tms320f28377d, and see my code working well in emulation mode.
I have changed my boot pins from default pins to GPIO148 and GPIO149 ( boot control register value : 0x94 95 ff 5a - verified it in memory if the value is correct in location 0x7801e ) using blinky_dcsm example and pulled them up to boot my CPU1 in GET/wait mode.
Anybody, what else should I do to make my application boot from internal flash.
Do I need to add any specific files in my project other than F2837xD_CodeStartBranch.asm
kindly help me out ASAP.
Regards,
Roshan tej thota