This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Champs,
As below description in F2806x datasheet for VDDIO:
Digital I/O and Flash Power Pin. Single supply source when VREG is enabled. Place a 2.2-uF decoupling capacitor on each pin. The exact value of the total decoupling capacitance should be determined by the system voltage regulation solution.
Customer needed to know whether that 2.2-uF is only the nominal value of the decoupling capacitor or that the decoupling capacitor should always be 2.2-uF during all operating temperature range.
Would you please kindly help? Thanks!
Best Regards,
Linda
Linda,
I presume you are looking at SPRS698F, not SPRS698G. The decoupling capacitor value should be chosen based on the application. Critical parameters to consider would be the total load connected to the 3.3v rail (i.e. in addition to the MCU itself), the board layout and the dynamic current requirement of the application.