This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm looking for the pin mux for the 100 pin version of the F28375D, I checked the online version and didn’t see it available.
Thanks,
Nick
Yes, I did two things to check this for you.
1. I checked the Datasheets for single and dual core for the 100 PZP package:
2. I checked the driverlib pin_map.h files for the two and they have identical content.
So yes. You should be able to use it without any issue. After I find and look at the design spec, if I find details that are not the same I will post the difference here for you.