This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I made New board. when i Started download program with my emulator(XDS200USB) :Code Composer Studio : Version: 6.2.0.00050
I checked GPIO for the Booting Mode( wait mode).
I have same problem in my hand . I have checked the watch window ,
plz, let me know, What should I do .! DO I need to Check other HW or SW Point??
Kim,
Adding to Ken's suggestions, please check below as well:
1. Check for updates in CCS and install them (especially TI C2000 Device support package, Debug Server Flash and any emulator packages).
2. Since you said it is a new custom board, check if there is any toggle on XRSn (reset) while loading the Flash. If the voltage lines are not up to the Datasheet spec level (during erase/program), Flash reads and erase/program can fail.
Thanks and regards,
Vamsi
Hi ken. Thank you for your reply.
I checked my project properties .
Like that. I have used this device since 2017. I checked sample program from TI( Blink LED) this program working in the ram area.
that is working well. but when I am loading Program in the Flash. that is not working as same.
I checked
1) voltage: VDD_IO(3.3V) and VDD core(1.2V). that is correct.
2) Check Mode GPIO( 72,84 ), when I change Mode( that is working as well. with XRS Pin: wait or SCI Mode)
DO I need to check other H/W(I/O, Same Item for Flash Writing ??)
If you have an Idea. Plz let me know.
-Kim
Kim,
Glad that upgrading to CCSv8 helped.
FYI for others that may refer to this post: All TMS320F2837x users should move to CCSv8 or CCSv9 (preferable) since the Flash Plugin is updated for the PCN (https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/729543?-FAQ-Product-Change-Notice-PCN-20180523001-1-for-TMS320F2837x-and-TMS320F2807x-devices) and the errata advisory "Flash: Minimum Programming Word Size".
Thanks and regards,
Vamsi