This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have a F28M36x controlCARD R1.1, with a F28M36P63C2ZWTT chip.
I have bricked the chip (C28 part), not sure how, but i cannot flash program it anymore. I have searched a lot of threads regarding the subject, and other people have had similar unresolveable issues.
Is it possible to replace only the F28M36P63C2ZWTT chip, since the rest of the board is fine? Can that be done okay and fairly easily?
Regards Niels
Niels,
It is definitely *possible*. “Fairly easily” is very subjective. This is a 289-Ball Fine Pitch Ball Grid Array package. While removal from the PCB is relatively easy, soldering the replacement device is harder and calls for considerable soldering expertise. If you have access to the resources (surface-mount soldering workstation and a technician highly skilled in removal/replacement of fine-pitch BGA parts), this is doable. You need to weigh in the cost of the replacement part plus the labor cost for removal/replacement and then make a call.