Hello,
I am using F28379D LaunchPad Development Kit for a project. I have design a simple circuit in the MATLAB simulink and run it in the F28379D LaunchPad Development Kit.
I am taking a AC signal input via ADC and providing it in DAC for output.
Both the input and output are seen in Oscilloscope.
There is a difference in Input signal and Output signal.
How can I make the output signal(DAC) more precise and close to Input signal (ADC)?
Which parameters of ADC and Simulink shall I change or modify in order to get a more precise output signal at DAC.
For easier understanding, I am providing some photos of the system.
Thanks in Advance.
The above photo is of the design in simulink.
The above photo is of the Parameters of the ADC.
The above photo is of the Parameters of the model and LaunchPad.
The above photo is of the Input Signal at ADC.
The above photo is of Output of DAC.
The above photo is both Input signal and Output signal.
I want to make the Yellow signal( Output of DAC) more precise to Green signal ( Input of ADC).