Part Number: TMS320F28377D
hi
I had loaded my codes into CPU1's RAM and CPU2's RAM,and both two CPU run properly.
also I loaded my codes into CPU1's FLASH and CPU2's FLASH,let two CPU run in STANDALONE mode,re-power the chip,both two CPU boot properly and begen to run.
But when I tired to load code to CPU1's ram ,use XDS100V2 debugging CPU1 and boot CPU2 from flash,I failed.
Please tell me what I should do?