This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Can I use XDS100V2 debugging CPU1 from RAM and at the same time, boot CPU2 from flash?

Part Number: TMS320F28377D

hi 

I  had loaded my codes into CPU1's RAM and CPU2's RAM,and both two CPU run properly.

also I  loaded my codes into CPU1's FLASH and CPU2's FLASH,let two CPU run in STANDALONE mode,re-power the chip,both two CPU boot properly and begen to run.

But when I tired to load code to CPU1's ram ,use XDS100V2 debugging CPU1 and boot CPU2 from flash,I failed.

Please tell me what I should do?