Hi,
if I move from 2755 to 2955 i see only thing that changes is the flash, just want to check can i just recompile code from 2755 on 2955 and if wasn't havn't issues before it should just recompile the same?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
if I move from 2755 to 2955 i see only thing that changes is the flash, just want to check can i just recompile code from 2755 on 2955 and if wasn't havn't issues before it should just recompile the same?
Thanks
It’s more whether it will run without problem without recompiling, for instance can just flash the 2955’s with the same 2755 code and recompiling will not be necessary, to save on time?
**Attention** This is a public forum