This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5329: Driving the XT2IN Clock Pin at 20MHz

Part Number: MSP430F5329
Other Parts Discussed in Thread: MSP-TS430PN80A

When driving the XT2IN with a crystal oscillator, what are the duty cycle specifications and the rise/fall times required?  Our existing oscillator is 20MHz with a 45% to 55% duty cycle and a 5nsec rise/fall times (when driving a 15pF).  A replacement oscillator is the same except the rise/fall times are 10nsec (when driving15pF).  Will this alternate crystal oscillator work with the MSP4305329?  Is there a minimum high time for the clock?  Is there a minimum low time for the clock?

**Attention** This is a public forum