This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430G2
I am attempting to program the MSP430FR2675 by using the MSP-EXP430G2 launch pad, I was told since both have SBW I should be able to accomplish this by hooking up the RST, VCC, VSS, and TEST pins from the launchpad to the FR2675 respectively. In code composer when I try flashing the chip it says it does not recognize the board. What other tool would I use to program the FR2675 chip?
Hi Alex,
Yes, this should work to program the FR2675 since SBW is supported. As Keith mentioned, be sure that you also have GND connected between the 2 boards.
Can you post a picture of your connections? Does the SBW work with the target on the launchpad?
Also note that the "Vcc" should be the 3.3 V rail and not the 5 V.
Good luck, I have one backordered at Digikey until January. However, any MSP430 Launchpad with SBW should work.
Alex,
The MSP-EXP430FR2433 appears to be in stock if you are not able to find the G2 ET board stocked somewhere.
https://www.ti.com/store/ti/en/p/product/?p=MSP-EXP430FR2433
**Attention** This is a public forum