Other Parts Discussed in Thread: MSP430FR5969
I have looked at two threads here dealing with similar Exit: 60, Verification Error issues but neither of them was of much help to me.
I am attempting to load a file (blink.hex) to an MSP430FR5969 through the MSP-FET, using MSP430Flasher, but am getting a Verification Error.
- The code is a simple led blink script that I have verified works. I loaded it through the board’s ez-fet debugger with mspdebug to verify.
Problem
I can load the Firmware.txt file that comes with the MSP430Flasher installation without an issue. But running my .hex file produces:
Exit: 60
ERROR: Verification Error
I am trying to figure out what makes one work while the other doesn’t.
The Successful Load vs The Unsuccessful Load
SUCCESS: Loading Firmware.txt with MSP430Flasher
Using the Firmware.txt file works perfectly:
MSP430Flasher.exe -e ERASE_ALL -w Firmware.txt -v -z [VCC]
Yields the result:

FAIL: Loading blink.hex with MSP430Flasher
I converted the blink executable to .hex with:
msp430-elf-objcopy -O ihex blink.o blink.hex
then attempt to load code with:
MSP430Flasher.exe -e ERASE_ALL -w blink.hex -v -z [VCC]
Yet get the output:

Thank you in advance.
Jazz Jackson