This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994: DMA Initialization using register based instructions for BOOST-XL Audio Playback project on MSP430FR5994

Part Number: MSP430FR5994


Hello everyone, 

I am trying to use the BOOST-XL Audio demo for an acoustic signal detection application via the MSP430FR5994 Launchpad. For the same, I have made some modifications to the 'audio_collect.c' sample file as provided in the MSPWare example. The idea behind this was to reduce the code size and try and find if there is an alternate way to code the behavior of the audio recording and playback. For initializing the DMA Channels to record and playback the audio, the original code is structured in the following way:

    static DMA_initParam dma0Config;
    static DMA_initParam dma1Config;

    dma0Config.channelSelect = DMA_CHANNEL_1;
    dma0Config.transferModeSelect = DMA_TRANSFER_SINGLE;
    dma0Config.transferSize = SAMPLES_LENGTH;
    dma0Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
    dma0Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
    dma0Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;
    
    dma1Config.channelSelect = DMA_CHANNEL_2;
    dma1Config.transferModeSelect = DMA_TRANSFER_SINGLE;
    dma1Config.transferSize = SAMPLES_LENGTH;
    dma1Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
    dma1Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
    dma1Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;
    
    DMA_init(&dma0Config);
    DMA_init(&dma1Config);

Instead of the above representation, my idea was to try out the following:

    #define ADC12_DMA_TRIGGER_SOURCE 0X1A   // (TRIGGER_SOURCE_26)
    #define SAMPLES_LENGTH 0x7FFF
    
    DMA1CTL = (DMADT_0 + DMADSTBYTE_0 + DMASRCBYTE_0 + DMALEVEL_0);
    DMA1SZ = SAMPLES_LENGTH;

    // Reset and then trigger the DMA Channel 1
    DMACTL1 &= 0X00FF;
    DMACTL1 |= (ADC12_DMA_TRIGGER_SOURCE << 8);
    
    DMA2CTL = (DMADT_0 + DMADSTBYTE_0 + DMASRCBYTE_0 + DMALEVEL_0);
    DMA2SZ = SAMPLES_LENGTH;
    
    // Reset and then trigger the DMA Channel 2
    DMACTL2 &= 0X00FF;
    DMACTL2 |= (ADC12_DMA_TRIGGER_SOURCE<<8);

While I have also used a similar idea for coding the behavior with the help of the registers, the entire code works when I use the initializations according to the 'DMA_initParam' but when I try to use the modified register based approach - the demo simply keeps recording the sound (the RED LED stays on) and never starts the playback. I am almost certain that the issue is in this fragment of code as when I use the default initializations for DMA while modifying the rest of the code according to a register based approach - the BOOST-XL demo works perfectly. I scouted the forum for similar questions but haven't seen one that applies in my case. If anyone could have a look at the code and let me know where I might be going wrong, it would be extremely helpful. I am also attaching the modified code file for the 'audio_collect.c' and the default sample as provided in the MSPWare for your reference. 

/* --COPYRIGHT--,BSD
 * Copyright (c) 2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//******************************************************************************
//!  TI-Design Signal Processing with LEA on MSP430FR5994
//!
//!  William Goh
//!  Texas Instruments Inc.
//!  April 2016
//******************************************************************************

//******************************************************************************
// Includes
//******************************************************************************
#include <stdlib.h>
#include <stdint.h>
#include <driverlib.h>
#include "audio_collect.h"
#include "global.h"
#include "dac8311.h"

#pragma LOCATION(dataRecorded1, 0x10000);
#pragma PERSISTENT(dataRecorded1);
uint16_t dataRecorded1[SAMPLES_LENGTH] = {0};

#pragma LOCATION(dataRecorded2, 0x20000);
#pragma PERSISTENT(dataRecorded2);
uint16_t dataRecorded2[SAMPLES_LENGTH] = {0};

//******************************************************************************
// Globals
//******************************************************************************
static DMA_initParam dma0Config;
static DMA_initParam dma1Config;

void runRecord(void)
{
    uint16_t recording = 0;

    P1OUT |= BIT0;

    // Initialize the microphone for recording
    gAudioConfig.bufferSize = SAMPLES_LENGTH;
    gAudioConfig.sampleRate = SAMPLING_FREQUENCY;
    Audio_setupCollect(&gAudioConfig);

    // Start the recording by enabling the timer
    Audio_startCollect(&gAudioConfig);

    recording = 1;

    while (recording){
        __bis_SR_register(LPM4_bits + GIE);

        recording = 0;
    }
}

//******************************************************************************
// Functions
//******************************************************************************
/* Function that powers up the external microphone and starts sampling
 * the microphone output.
 * The ADC is triggered to sample using the Timer module
 * Then the data is moved via DMA. The device would only wake-up once
 * the DMA is done. */
void Audio_setupCollect(Audio_configParams * audioConfig)
{
    // Turn on mic power full drive strength and enable mic input pin to ADC
    MIC_POWER_PORT_OUT |= MIC_POWER_PIN;
    MIC_POWER_PORT_DIR |= MIC_POWER_PIN;

    AUDIO_PORT_SEL0 |= MIC_INPUT_PIN;
    AUDIO_PORT_SEL1 |= MIC_INPUT_PIN;

    // For safety, protect RMW Cpu instructions
    DMACTL4 |= DMARMWDIS;

    // Initialize the DMA. Using DMA channel 1.
//    dma0Config.channelSelect = DMA_CHANNEL_1;
//    dma0Config.transferModeSelect = DMA_TRANSFER_SINGLE;
//    dma0Config.transferSize = SAMPLES_LENGTH;
//    dma0Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
//    dma0Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
//    dma0Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;


    DMA1CTL = (DMADT_0 + DMADSTBYTE_0 + DMASRCBYTE_0 + DMALEVEL_0);
    DMA1SZ = SAMPLES_LENGTH;

    DMACTL1 &= 0X00FF;
    DMACTL1 |= (ADC12_DMA_TRIGGER_SOURCE << 8);

    // Initialize the DMA. Using DMA channel 2.
//    dma1Config.channelSelect = DMA_CHANNEL_2;
//    dma1Config.transferModeSelect = DMA_TRANSFER_SINGLE;
//    dma1Config.transferSize = SAMPLES_LENGTH;
//    dma1Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
//    dma1Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
//    dma1Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;
////

    DMA2CTL = (DMADT_0 + DMADSTBYTE_0 + DMASRCBYTE_0 + DMALEVEL_0);
    DMA2SZ = SAMPLES_LENGTH;
////
    DMACTL2 &= 0X00FF;
    DMACTL2 |= (ADC12_DMA_TRIGGER_SOURCE<<8);

//    DMA_init(&dma0Config);
//    DMA_init(&dma1Config);

    __data16_write_addr((unsigned short) &DMA1SA, (uint32_t) &ADC12MEM0);
    DMA1CTL &= ~(DMASRCINCR_3);    // DMA channel 1 reset source increment bits before setting them
    DMA1CTL |= DMASRCINCR_0;       // DMA channel 1 Source address is unchanged

    __data16_write_addr((unsigned short) &DMA1DA, (uint32_t) &dataRecorded1);
    DMA1CTL &= ~(DMADSTINCR_3);    // DMA channel 1 reset dest increment bits before setting them
    DMA1CTL |= DMADSTINCR_3;       // DMA channel 1 Dest address is incremented

    __data16_write_addr((unsigned short) &DMA2SA, (uint32_t) &ADC12MEM0);
    DMA2CTL &= ~(DMASRCINCR_3);    // DMA channel 2 reset source increment bits before setting them
    DMA2CTL |= DMASRCINCR_0;       // DMA channel 2 Source address is unchanged

    __data16_write_addr((unsigned short) &DMA2DA, (uint32_t) &dataRecorded2);
    DMA2CTL &= ~(DMADSTINCR_3);    // DMA channel 2 reset dest increment bits before setting them
    DMA2CTL |= DMADSTINCR_3;       // DMA channel 2 Dest address is incremented


    // Configure ADC
    ADC12CTL0 &= ~ADC12ENC;           // Disable conversions to configure ADC12
    // Turn on ADC, sample 32 clock cycles =~ 2us
    ADC12CTL0 = ADC12ON + ADC12SHT0_3;

    // Use sample timer, rpt single chan 0, use MODOSC, TA0 timer channel 1
    ADC12CTL1 = ADC12SHP + ADC12CONSEQ_2 + ADC12SHS_1;

    // Mic input to ADC, (AVCC/AVSS ref), sequence end bit set
    ADC12MCTL0 = MIC_INPUT_CHAN | ADC12EOS;

    // Initialize Timer_A channel 1 to be used as ADC12 trigger
    // Initialize TACCR0 (period register) 8MHz/20kHz = 400
    // Simple counter with no interrupt. 0...400 = 400 counts/sample

//    // Initialize TA0CCR1 to generate trigger clock output, reset/set mode
    TA0CTL &= ~(TASSEL + MC + TACLR + TAIE + ID);
    TA0EX0 &= ~TAIDEX;
    TA0EX0 |= TAIDEX_0;
    TA0CTL |= (TASSEL__SMCLK + TACLR);
    TA0CCTL0 &= ~CCIE;
    //TA0CCR0 = (__SYSTEM_FREQUENCY_MHZ__ / config->sampleRate) - 1;
    TA0CCR0 = 499;

    // Initialize Timer_A0 channel 1 (toggle reset) to be used as ADC12 trigger
    // Initialize TA0CCR1 to generate trigger clock output, reset/set mode
    TA0CCTL1 &= ~CAP;
    TA0CCTL1 &= ~(CCIE + OUTMOD);
    TA0CCTL1 |= OUTMOD_2;
    //TA0CCR1 = ((__SYSTEM_FREQUENCY_MHZ__ / config->sampleRate) / 2) - 1;
    TA0CCR1 = 249;

    // Enable ADC to convert when a TA0 edge is generated
    ADC12CTL0 |= ADC12ENC;

    // Delay for the microphone to settle
    __delay_cycles(10000);
}

/*--------------------------------------------------------------------------*/
/* Start collecting audio samples in ping-pong buffers */
void Audio_startCollect(Audio_configParams * audioConfig)
{
    // Enable DMA channel 1 interrupt
    DMA1CTL |= DMAIE;

    // Enable the DMA0 to start receiving triggers when ADC sample available

    DMA1CTL |= DMAEN;


    // Start TA0 timer to begin audio data collection
    TA0CTL |= TACLR;
    TA0CTL |= MC_1;

}

/*--------------------------------------------------------------------------*/
/* Stop collecting audio samples in buffers */
void Audio_stopCollect(Audio_configParams * audioConfig)
{

    TA0CTL &= ~MC;

    if(~(ADC12CTL1_L & ADC12CONSEQ_3))
        {
            //To prevent preemption of a single-channel, single-conversion we must
            //wait for the ADC core to finish the conversion.
            while(ADC12CTL1_L & ADC12BUSY)
            {
                ;
            }
        }
        ADC12CTL0_L &= ~(ADC12ENC);

    // Disable DMA channel and interrupt
    DMA1CTL &= ~DMAEN;
    DMA1CTL &= ~DMAIE;

    // Disable DMA channel and interrupt
    DMA2CTL &= ~DMAEN;
    DMA2CTL &= ~DMAIE;


}

/*--------------------------------------------------------------------------*/
/* Shut down the audio collection peripherals*/
void Audio_shutdownCollect(Audio_configParams * audioConfig)
{
    // Turn off preamp power
    MIC_POWER_PORT_OUT &= ~MIC_POWER_PIN;

    // Disable the ADC
    ADC12CTL0_L &= ~ADC12ENC;
    ADC12CTL0_L &= ~ADC12ON;

    // delay of 10 ms to let mic go in WoS mode completely
//    __delay_cycles(0.010 * __SYSTEM_FREQUENCY_MHZ__);

}
     
/* --COPYRIGHT--,BSD
 * Copyright (c) 2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//******************************************************************************
//!  TI-Design Signal Processing with LEA on MSP430FR5994
//!
//!  William Goh
//!  Texas Instruments Inc.
//!  April 2016
//******************************************************************************

//******************************************************************************
// Includes
//******************************************************************************
#include <stdlib.h>
#include <stdint.h>
#include <driverlib.h>
#include "audio_collect.h"
#include "global.h"
#include "dac8311.h"

#pragma LOCATION(dataRecorded1, 0x10000);
#pragma PERSISTENT(dataRecorded1);
uint16_t dataRecorded1[SAMPLES_LENGTH] = {0};

#pragma LOCATION(dataRecorded2, 0x20000);
#pragma PERSISTENT(dataRecorded2);
uint16_t dataRecorded2[SAMPLES_LENGTH] = {0};

//******************************************************************************
// Globals
//******************************************************************************
static DMA_initParam dma0Config;
static DMA_initParam dma1Config;

void runRecord(void)
{
	uint16_t recording = 0;

	P1OUT |= BIT0;

	// Initialize the microphone for recording
	gAudioConfig.bufferSize = SAMPLES_LENGTH;
	gAudioConfig.sampleRate = SAMPLING_FREQUENCY;
	Audio_setupCollect(&gAudioConfig);

	// Start the recording by enabling the timer
	Audio_startCollect(&gAudioConfig);

	recording = 1;

	while (recording){
		__bis_SR_register(LPM4_bits + GIE);

		recording = 0;
	}
}

//******************************************************************************
// Functions
//******************************************************************************
/* Function that powers up the external microphone and starts sampling
 * the microphone output.
 * The ADC is triggered to sample using the Timer module
 * Then the data is moved via DMA. The device would only wake-up once
 * the DMA is done. */
void Audio_setupCollect(Audio_configParams * audioConfig)
{
    Timer_A_initUpModeParam upConfig =
    {
        TIMER_A_CLOCKSOURCE_SMCLK,
        TIMER_A_CLOCKSOURCE_DIVIDER_1,
        (__SYSTEM_FREQUENCY_MHZ__ / audioConfig->sampleRate) - 1,
        TIMER_A_TAIE_INTERRUPT_DISABLE,
        TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE,
        TIMER_A_DO_CLEAR,
        false
    };

    Timer_A_initCompareModeParam compareConfig =
    {
        TIMER_A_CAPTURECOMPARE_REGISTER_1,
        TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE,
        TIMER_A_OUTPUTMODE_TOGGLE_RESET,
        ((__SYSTEM_FREQUENCY_MHZ__ / audioConfig->sampleRate) / 2) - 1
    };

    // Turn on mic power full drive strength and enable mic input pin to ADC
    MIC_POWER_PORT_OUT |= MIC_POWER_PIN;
    MIC_POWER_PORT_DIR |= MIC_POWER_PIN;

    AUDIO_PORT_SEL0 |= MIC_INPUT_PIN;
    AUDIO_PORT_SEL1 |= MIC_INPUT_PIN;

    // For safety, protect RMW Cpu instructions
    DMA_disableTransferDuringReadModifyWrite();

    // Initialize the DMA. Using DMA channel 1.
    dma0Config.channelSelect = DMA_CHANNEL_1;
    dma0Config.transferModeSelect = DMA_TRANSFER_SINGLE;
    dma0Config.transferSize = SAMPLES_LENGTH;
    dma0Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
    dma0Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
    dma0Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;


    // Initialize the DMA. Using DMA channel 2.
    dma1Config.channelSelect = DMA_CHANNEL_2;
    dma1Config.transferModeSelect = DMA_TRANSFER_SINGLE;
    dma1Config.transferSize = SAMPLES_LENGTH;
    dma1Config.triggerSourceSelect = DMA_TRIGGERSOURCE_26;
    dma1Config.transferUnitSelect = DMA_SIZE_SRCWORD_DSTWORD;
    dma1Config.triggerTypeSelect = DMA_TRIGGER_RISINGEDGE;

	DMA_init(&dma0Config);
    DMA_init(&dma1Config);

    DMA_setSrcAddress(DMA_CHANNEL_1,
                      (uint32_t) &ADC12MEM0,
                      DMA_DIRECTION_UNCHANGED);

    DMA_setDstAddress(DMA_CHANNEL_1,
                      (uint32_t) (&dataRecorded1),
                      DMA_DIRECTION_INCREMENT);

    DMA_setSrcAddress(DMA_CHANNEL_2,
                      (uint32_t) &ADC12MEM0,
                      DMA_DIRECTION_UNCHANGED);

    DMA_setDstAddress(DMA_CHANNEL_2,
                      (uint32_t) (&dataRecorded2),
                      DMA_DIRECTION_INCREMENT);

    // Configure ADC
    ADC12CTL0 &= ~ADC12ENC;           // Disable conversions to configure ADC12
    // Turn on ADC, sample 32 clock cycles =~ 2us
    ADC12CTL0 = ADC12ON + ADC12SHT0_3;

    // Use sample timer, rpt single chan 0, use MODOSC, TA0 timer channel 1
    ADC12CTL1 = ADC12SHP + ADC12CONSEQ_2 + ADC12SHS_1;

    // Mic input to ADC, (AVCC/AVSS ref), sequence end bit set
    ADC12MCTL0 = MIC_INPUT_CHAN | ADC12EOS;

    // Initialize Timer_A channel 1 to be used as ADC12 trigger
    // Initialize TACCR0 (period register) 8MHz/20kHz = 400
    // Simple counter with no interrupt. 0...400 = 400 counts/sample
    Timer_A_initUpMode(TIMER_A0_BASE, &upConfig);

    // Initialize TA0CCR1 to generate trigger clock output, reset/set mode
    Timer_A_initCompareMode(TIMER_A0_BASE, &compareConfig);

    // Enable ADC to convert when a TA0 edge is generated
    ADC12CTL0 |= ADC12ENC;

    // Delay for the microphone to settle
    __delay_cycles(10000);
}

/*--------------------------------------------------------------------------*/
/* Start collecting audio samples in ping-pong buffers */
void Audio_startCollect(Audio_configParams * audioConfig)
{
    // Enable DMA channel 1 interrupt
    DMA_enableInterrupt(DMA_CHANNEL_1);

    // Enable the DMA0 to start receiving triggers when ADC sample available
    DMA_enableTransfers(DMA_CHANNEL_1);

    // Start TA0 timer to begin audio data collection
    Timer_A_clear(TIMER_A0_BASE);
    Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_UP_MODE);
}

/*--------------------------------------------------------------------------*/
/* Stop collecting audio samples in buffers */
void Audio_stopCollect(Audio_configParams * audioConfig)
{
    Timer_A_stop(TIMER_A0_BASE);

    ADC12_B_disableConversions(ADC12_B_BASE, ADC12_B_COMPLETECONVERSION);

    // Disable DMA channel and interrupt
    DMA_disableTransfers(DMA_CHANNEL_1);
    DMA_disableInterrupt(DMA_CHANNEL_1);

    // Disable DMA channel and interrupt
    DMA_disableTransfers(DMA_CHANNEL_2);
    DMA_disableInterrupt(DMA_CHANNEL_2);
}

/*--------------------------------------------------------------------------*/
/* Shut down the audio collection peripherals*/
void Audio_shutdownCollect(Audio_configParams * audioConfig)
{
    // Turn off preamp power
    MIC_POWER_PORT_OUT &= ~MIC_POWER_PIN;

    // Disable the ADC
    ADC12_B_disable(ADC12_B_BASE);
}
   

Let me know if any other details are necessary. Thanks!

Regards,

Siddhant 

  • I'm not very familiar with this board, but I notice a few things:

    -------------

    DMA1TSEL is in DMACTL0, not DMACTL1 [Ref User Guide (SLAU367P) Table 11-5]

    -------------

    >DMACTL2 &= 0X00FF;
    >DMACTL2 |= (ADC12_DMA_TRIGGER_SOURCE<<8);

    DMA2TSEL is the low byte of DMACTL1 [Ref user guide  Table 11-6]

    >DMACTL1 &= 0XFF00;
    >DMACTL1 |= (ADC12_DMA_TRIGGER_SOURCE<<0);

    -------------

    > __data16_write_addr((unsigned short) &DMA2SA, (uint32_t) &ADC12MEM0);

    DMA2SA (and DA) is 20 bits wide (really 32 bits), so I suggest something more like:

    > __data20_write_long((uintptr_t)&DMA2SA, (uintptr_t)&ADC12MEM0); 

    -------------

    It might be useful to pause the original program, then write down the interesting DMA registers in the Registers View and compare them to the values you get with your code. It might be quicker than inspection, anyway.

  • Hey Bruce, 

    Thanks! I will take a look and update the issue here accordingly.

**Attention** This is a public forum