Part Number: EVM430-FR6043
hi everyone
i have trouble with my EVM430-FR6043 to connect with the HID device over the USS SW.
my setup is on windows 10 ccs Version: 11.0.0.00012, USS_02_40.
i can build and load the USS_Water_Demo to the MCU, but i cant connect with the USS SW to the HID device. "HID device detected, but could not connect to it"
the device manager shows MSP Application UART1 (COM1) and MSP Debug Interface (COM4).
What im missing or what could help? (i tried it with a VM on Windows 7 and there it worked, but i limmited ressources there)
Thanks for any ideas