This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using MSP430F5xx_6xx driverlib Version 2.91.13.01 for MSP430F5510. We need to generate a BOR from S/W but we noticed that the PMM_trigBOR API does not exist on this device even though the associated PMM register bits exist in H/W.
Questions:
HWREG16(PMM_BASE + OFS_PMMCTL0) |= PMMSWBOR;
HWREG8(PMM_BASE + OFS_PMMCTL0_H) = PMMPW_H; HWREG8(PMM_BASE + OFS_PMMCTL0) |= PMMSWBOR; HWREG8(PMM_BASE + OFS_PMMCTL0_H) = 0x00;
The driverlib source for MSP430FR5xx_6xx implements the function as shown in 3b but I'm thinking a 16bit write as shown in 3a should be sufficient.
Thanks
Hello,
What you have proposed should work to trigger a BOR via the PMM. You would need to change your coding though to incorporate the PMMPW for the register. So you would want to do word access, and provide the PMMPW + PMMSWBOR. PMMSWBOR would be low byte btw.
So something like: -- assuming PMMPW is defined via driverlib
/// DriverLib Style HWREG16(PMM_BASE + OFS_PMMCTL0) |= (PMMPW + PMMSWBOR); /// Register Level PMMCTL0 |= (PMMPW + PMMSWBOR);
Assuming you have the standard MSP430 header files linked, I also included a register level example of doing this.
Thanks! I was getting a reset without a password but this is the PUC that results from writing the incorrect password. I've fixed this now to get the desired POR.
**Attention** This is a public forum