Part Number: MSP-EXP430F5529LP
Other Parts Discussed in Thread: MSP430F5529, UNIFLASH, ENERGIA, MSP-FET, MSP-FLASHER, MSP430F5528
Hi everybody,
I have a new MSP-EXP430F5529LP board, but I can't get it to work.
Connecting the EVM to the PC via USB, I should see 2 new COM ports appear in the devices tree:
- MSP Application UART1
- MSP Debug Interface
Actually, after enumeration, I don't see these two ports, but only 4 new HID elements (all with VID=2047 and PID=0200):
- n.2 "HID-compliant vendor-defined device"
- n.2 "USB Input Device"
The result is this:
- both LEDs connected to the eZ-FET emulator on the board remain off
- both LEDs connected to the MSP430F5529 remain off
- all the tools that I tried like CCS, Energia and UniFlash fail to connect to the emulator reporting the error "Error initializing emulator: No USB FET was found"
I initially followed the "SLAU533D - MSP430F5529 LaunchPad Development Kit" document and then I searched for more information on this forum, but without success so far.
I also downloaded and installed the low-level USB drivers (“ti_msp430driver_setup_1.0.1.2-windows”).
The PC used for these tests runs on Windows 10, I've done some tests also on Windows XP and Windows 7, but I don't get any improvement.
It would be great if you could give me some advice, thanks in advance.
Kind regards,
Marco