Part Number: MSP430FR5729
I try to configure a clock scheme as: "crystal oscillator 20MHz -> XTAL1 -> SMCLK". Divider I set to 4.
The program with the code that I configure a clock and the crystal connection scheme is below. I expect take a 5 MHz at the SMCLK out pin (PJ.0), but the 1.22 MHz I having in result. I don't understand why and very do hope for advice why it may be.
#include <msp430.h>
#ifndef __DATATYPES_H__
#define __DATATYPES_H__
typedef char int8_t;
typedef unsigned char uint8_t;
typedef int int16_t;
typedef unsigned int uint16_t;
typedef long int32_t;
typedef unsigned long uint32_t;
typedef uint8_t BYTE;
#endif
/**
* main.c
*/
inline void __ClkConf(void);
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
__ClkConf();
while(1)
{
}
return 0;
}
inline void __ClkConf(void)
{
uint16_t temp;
PJSEL0 |= BIT0;
PJSEL1 &= ~((uint16_t)BIT0);
PJDIR |= BIT0 + BIT4 + BIT5;
PJOUT |= BIT0 + BIT4 + BIT5;
PJSEL0 |= BIT4 + BIT5; // connect pins to xtal;
CSCTL0_H = 0xA5;
CSCTL1 |= DCOFSEL0 + DCOFSEL1; // Set max. DCO setting
CSCTL2 = SELA_3 + SELS_0 + SELM_3; // set ACLK = MCLK = DCO; SMCLK = XTAL1
CSCTL3 = DIVA_0 + DIVS_2 + DIVM_0; // set all dividers
temp = CSCTL4;
temp |= XTS;
temp &= ~(XT1OFF);
CSCTL4 = temp;
}