This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm able to run the simple blink LED program with a MSP430FR4133 installed to the board, however, I cannot repeat with the MSP430F2418 example project. I've tried several samples of the 2418 and CCS returns with a connection error: Unknown device every time.
Using JTAG jumpers on the MSP-TS430PM64D board.
3.3V from the MSP-FET is ok.
Win 10 running on a HP Z-book.
Tried restarting CCS, laptop, MSP-FET. No improvements.
Any suggestions?
Hi
this is the connection between MSP-FET to target device issue.
Checke the product page of MSP430F2418, MSP-TS430PM64 baord shoud be used for F2418. MSP-TS430PM64D board is for FR4133 device.
So, Please check the spec of these 2 socket board and maybe you need using MSP-TS430PM64 baord for F2418 debug.
Thanks!
Thank you for your advice, my M64 arrived and my 2418 is working great now. Thanks again!
**Attention** This is a public forum