Hi team,
Here's an issue from the customer may need your help:
When using filter_ex2_fir_iq31 routine to debug, it will stuck in the the below statement of Zero initialize the output buffer:
while(count--) WRITE8_ADV(outbuf, 0)
/*------------------------------------------------------------------------*/
/* Zero initialize the output buffer. */
/*------------------------------------------------------------------------*/
#if __MSP430__
while(count--) WRITE8_ADV(outbuf, 0);
#else
if (USE_MEMSET)
memset((void*)outbuf, 0, count);
else
while(count--) WRITE8_ADV(outbuf, 0);
#endif
}
Please see the following debugging window:
Could you help check this case? Thanks.
Best Regards,
Cherry