Part Number: MSP430F5358
Other Parts Discussed in Thread: MSP-FET, , TMP468, MSP430F6459
Hello TI team,
I want to flash my MSP through BSL UART using MSP-FET, below is my pin connection.
MSP-FET | MSP430F5358
PIN8-TEST | TEST/SBWTCK
PIN9-GND | GND
PIN11-RST | RST#/NMI/SBWTDIO - RST
PIN12-Tx | P1.1-TX
PIN14-Rx | P1.2-RX
Running through CMD below command,
BSLDEMO-2.01c.exe -cCOM37 <source dir>\Debug/tmp468.txt
Getting below Failed condition.
MSP430 Bootstrap Loader Communication Program (Version 2.01c)
Mass Erase...
ERROR: Synchronization failed!
Device with boot loader connected?
Is the pin connection correct? What is missing the making it fail?
Thanks,
Shubhanshu