Dear Team,
Hope you are doing well.
I got a question from the customer during the use of MSP430G2755.
They found that some G2755 malfunctioned:
1.Less than 10 seconds after powered G2755, the G2755 was failed to run the main program. (The initializer program can be run normally before the G2755 went wrong.)
2. When G2755 went wrong, if used the Reset pin to reset G2755 or cut off the power and turned on the power immediately, the G2755 could work normally after both actions. (If cut off the power but not turned on the power again in about 15 minutes, G2755 would still fail to run the program )
3. The failure occurred only after the first time powering the G2755. If the failure occurred, cut off and repower the G2755, the G2755 can run normally.
4. Customer had tried to change the faulty G2755 from one machine to the other, and with the faulty G2755, the other machine also had the same problem.
5. Changed different program to input to the faulty G2755, it still did not work in normal. But if use the same program input to G2755 that worked in normal, the program can be run.
6. The customer used external oscillator, the G2755 failed to drive external oscillator in some cases.
Please help to analyze what may cause this issue and how to solve.
Really appreciate your help!
Best regards,