Other Parts Discussed in Thread: MSP430F5529,
Hello,
It is recommended to connect a 1MΩ resistor to ground on pin 63 (PUR) of the MSP430F5529 if the USB interface is not used. Can this resistor also be placed on the same pin of the MSP430F5329 without impacting performance or functionality? The MSP430F5329 lists this pin as NC, but we would prefer a single layout for both microcontrollers.
Thanks