This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET: Error initializing emulator: Interface Communication Error

Part Number: MSP-FET
Other Parts Discussed in Thread: MSP-EXP430FR5969

I have an MSP-FET that I have been using for some time, but it has recently stopped working. When attempting to program a microcontroller through Code Composer Studio, I receive the following error: "Error initializing emulator: Interface Communication error". 

I was able to borrow another MSP-FET from a colleague which worked immediately with no issues. The PC, USB cable, FET ribbon cable, target board (MSP-EXP430FR5969) and software (blink.c) were all kept the same, so I am certain that the error is with the MSP-FET itself. I have tried performing a HID cold boot as per the MSP Debuggers User's Guide which allowed me to successfully re-flash the device firmware, but it still presents the same error message. I have also confirmed that this is the same firmware that is loaded on the working device.

Are there any further steps I can take to identify the source of the error and hopefully recover the device? I would obviously prefer to recover my existing FET rather than purchasing a new one if at all possible. If any further info is required please let me know.

**Attention** This is a public forum