Hi,
From the below image which bootloader file support for MSP430F5310. Please clarify it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
From the below image which bootloader file support for MSP430F5310. Please clarify it.
MSP430F4310 is using the image below
You can find it at the folder named ...\MSP430BSL_1_02_00_01\Released_BSL_Images\MSP430F532x_534x_530x_Family\
Hi Nidheesh,
I think you can refer to the demo
...\MSP430BSL_1_02_00_01\IAR_BSL_Source\IAR_v6_MSP430F543xA_TA_UART
Best regards
Gary
You can try this project
...\MSP430BSL_1_02_00_01\CCS_BSL_Source\CCS_v7_MSP430F543xA_TA_UART
Can I get CCS IDE supported source code for ...\MSP430BSL_1_02_00_01\Released_BSL_Images\MSP430F532x_534x_530x_Family\ this BSL image .?
No, I can't find such source code. But it should works with project I point to you.
Yes, I have mentioned before as below
...\MSP430BSL_1_02_00_01\IAR_BSL_Source\IAR_v6_MSP430F543xA_TA_UART
**Attention** This is a public forum