This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5328: MSP430F5328

Part Number: MSP430F5328

Hi TI teams,

 May I ask one question about msp430f5328 BSL? I want to customize the BSL source code project for MSP430F5328 to implement our firmware upgrade. Cause our application image size already more than half of the internal flash, so we need to add a external flash to manage the image backup or crc check etc.,the external flash connected to MCU through SPI, can I add SPI external flash read/write logic to BSL? and will the SPI read/write can working properly in BSL? 

Another, if BSL cannot do this, can I use MSPboot to do this? Currently there is no MSPboot example for MSP430F5328, if I want to customize it, is it possible? Thank you very much.

Best Regrads,

Thank you

**Attention** This is a public forum