Hi,
Good Day.
The customer is working with the EVM430-FR6047 board to measure the flow rate in a pipe. He is wondering if it is capable of detecting ranges around 17GPM or 25GPM.
He knows it is kind of specific but on the online documentation it was not clear on the upper limits of its capability.
He is using 1MHz sensors and the signal that is picked up is very poor. Even after changing the parameters around it doesn't look good so he was wondering if it wasn't able to handle the flow rate.
Please advise. Thank you very much.
Best Regards,
Ray Vincent