Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP-FET, UNIFLASH
I have been unable to get any response out of the evaluation kit or the launchpad after flashing the latest firmware to them. There is no communication on the UART, no LCD response, and no LEDs. (Only the launchpad blinks)
I've uploaded the following into the EVM430: "C:\ti\msp\EnergyMeasurementDesignCenter_1.40.00.03\EnergyMeasurementDesignCenter\example_projects\EnergyMeasurementDesignCenterWorkspace\EVM430-F6779_CT_3V_3C_60Hz\EVM430-F6779_CT_3V_3C_60Hz.txt"
And the following into the launchpad: "C:\ti\msp\EnergyMeasurementDesignCenter_1.40.00.03\EnergyMeasurementDesignCenter\hidbridge\TI_MSP_HIDBRIDGE__1_00_04_00__MSP-EXP430F5529LP.txt"
The launchpad shows the slow blinking LED, and the Energy Measurement Design Center is able to connect to the launchpad correctly. But there is NO communication across the UART except when unchecking "Connected" in the controller properties.
At this time, only Line 3 of the EVM is connected to a standard 120V outlet for availability and convenience reasons. Otherwise, I would have to spend all of my time in the cold warehouse. The out-of-box firmware worked in this configuration and gave accurate voltage and wattage output, so I expected it to work with the updated EMDC firmware.
I've double checked the connections for the UART according the documentation, and ran through the steps at least twice. The MSP-FET is able to connect to and flash the EVM, but nothing happens.
Is there something I'm missing here?