Part Number: MSP430AFE253
Hi team,
Here's an issue from the customer may need your help:
When SD24GAINx is set to 0 time in the program, the exact voltage value can be calculated correctly using the formula (ad value / 7fff)*0.6V.
The customer now want to reduce the range -0.6V to 0.6V. Is it possible by modify SD24GAINx to achieve this? If so, set SD24GAIN x to 011 or x8. How much does 0.6 in the calculation formula (ad/7fff)*0.6 need to be modified?
They've tried 0.075 but there was a deviation. Around 0.0772 is probably correct. Why is that? Is the deviation from using the gain? Or is it not possible to implemented by this way?
Could you help check this case? Thanks.
Best Regards,
Cherry