Part Number: MSP430AFE253
Tool/software:
Hi team!
I've been testing the SD24 in MSP430AFE253, and trying to use in an application which requires to fetch an approximately 0.08 mV signal with msp. However during my test, neither using the channel 7(which is short-circuit internally) nor pasting both pins in an tin ball could make the output stable. It seems that sampling with SD24 is always mixed with a noise of approximate 0.1 mV Vp-Vp.
My question is, is it unavoidable?(which means a few bits of the LSB are meaningless) Or does the changing data actually reflects the voltage on the short-circult pins? Or are they produced because of the ADC's sampling logic itself? What should I do to reduce the noise(if they are really NOISE)?
FYI, fm=921.6kHz, OSR=256, fs = 3.6kHz. Setting high impedance input buffer on or off may have little influence on the Vp-Vp voltage, but none of them could fix the restless data.


fig.1 data collected during about 4 s.
fig.2 data zoomed in focusing on a duration of 0.2 s.
Thanks for any help!
Best regards,
Ceiliusion