Other Parts Discussed in Thread: TIDM-3OUTSMTSTRP, TIDM-TWOPHASEMETER-I2040
Hello,
I am working on a design that utilizes an MSP430I2021. In this design, an analog signal proportional to a temperature reading is connected to A0.0+ with respect to A0.0-. I am utilizing an external 1.25 Volt reference that is applied to VREF with respect to AVSS. The pins A0.0-, AVSS, and DVSS are all tied to the same node.
Note 2 in section 8.7.7.4 on page 22 of the datasheet for the MSP430I2021 indicates that the acceptable full-scale input range should be:
-0.8 * VREF / GAIN to 0.8 * VREF / GAIN
With a GAIN of 1 and a VREF of 1.25, this corresponds to an acceptable input range of -1 VDC to +1 VDC. Under normal operation, staying within this operating range will not be an issue. However, out-of-range temperatures and sensor failures could cause the potential on pin A0.0+ with respect to pins A0.0-, AVSS, and DVSS to drift outside of this range for an indefinite amount of time.
What are the positive and negative limits of the potential that can be applied to pin A0.0+ with respect to pins A0.0-, AVSS, and DVSS without damaging the MSP430I2021?
The datasheet referenced in this message is attached for convenience.