Greetings everyone,
I'm currently working with the EVM430 F6779 and I am attempting to retrieve data through the UART pin as shown in the image below:
Initially, I was able to successfully retrieve the data. However, the following day, upon turning on the meter, I was unable to see any data on the screen and the LEDs remained on. I have been troubleshooting for two months now, but have yet to find a solution.
Given the length of time I've been working on this issue without success, it's possible that there may be a hardware problem causing the problem. If there is anyone in this community who has expertise in this area and can offer assistance, I would greatly appreciate it.
I would also appreciate any insights or advice that anyone in this community might have to offer. Thank you in advance for your assistance!