Hello,
I'm using an MSP430F5310 microcontroller and I am trying to verify that the XT1CLK oscillator peripheral is indeed using the external 32.768 crystal, and not REFO. Is there a way to do this? I hand soldered a 40kHz crystal to the XT1 pins, and ACLK still shows 32.768kHz. Is this right? How can you prove out that XT1CLK is in fact using the external 32.768kHz crystal, and not an internal 32.768kHz one?