This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULC1001-DRV290XEVM: loading firmware to the msp430 using UniFlash

Part Number: ULC1001-DRV290XEVM

I am trying to connect to the msp430 to upload firmware. However I do not think the msp430 is connecting. I am plugged into the J3 micro-usb port. The firmware provided by TI is giving multiple errors about not being able to open source files. Is this because I am not connected to the msp430?

  • Hi Tyler,

    Sorry for late response, the holiday just ended.

    I have gone through the instructions of XEVM, and I have NOT found the msp430 device in the EVM. So, what part number of the msp430 you are loading firmware to? and what is the connection between the msp430 and the XEVM board.

    B.R.

    Sal

**Attention** This is a public forum