This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP low-power microcontroller forum

Part Number: MSP-GANG
Other Parts Discussed in Thread: MSP430F6459

I am working with MSP-Gang programmer for the programming fixture for MSP430F6459.

I am facing some problem, the MSP-Gang does not able to perform programming, I perform a selftest, there is error as below.

207: Image Flash Access (get ID) 0x0002 (0x0001 - 0x0003) Result: 0x00 ... >> ERROR <<
217: TEST Fuse keys (#1 ON) 1.00 ( 0.80 to 3.00) Result: 0.69 ... >> ERROR <<
218: TEST Fuse keys (#2 ON) 2.00 ( 0.80 to 3.00) Result: 0.64 ... >> ERROR <<
219: TEST Fuse keys (#3 ON) 3.00 ( 0.80 to 3.00) Result: 0.66 ... >> ERROR <<
220: TEST Fuse keys (#4 ON) 4.00 ( 0.80 to 3.00) Result: 0.67 ... >> ERROR <<
221: TEST Fuse keys (#5 ON) 5.00 ( 0.80 to 3.00) Result: 0.68 ... >> ERROR <<
222: TEST Fuse keys (#6 ON) 6.00 ( 0.80 to 3.00) Result: 0.68 ... >> ERROR <<
223: TEST Fuse keys (#7 ON) 7.00 ( 0.80 to 3.00) Result: 0.69 ... >> ERROR <<
224: TEST Fuse keys (#8 ON) 8.00 ( 0.80 to 3.00) Result: 0.68 ... >> ERROR << 

After few rounds of reset, the error seems to be disappear, but i am still having problem to perform programming, the error 33 IR Communication failed.

We replace with another MSP-Gang Programmer, we are able to perform programming without error.
Your help is very much appreciated.

CS1887400

**Attention** This is a public forum