Other Parts Discussed in Thread: EVM430-F6779, UNIFLASH, MSP-EXP430F5529LP
Hi team,
I am working on the EMDC and EVM430-F6779.
I followed the guidelines (From Design Center GUI) and programmed the HID bridge which is the MSP-EXP430F5529LP using the UniFlash connected to the GUI. I can only see the text "HID Connected" at the bottom left of the GUI in EMDC.
but in the setup guide it is showing as
I tried multiple steps but didn't get the above mentioned display.
I tried to check the results below is mentioned in the guidelines
the below is the what it displayed to me
checking the results tab in guidelines it is shown as below
for me it is showing empty tabs as below
this below is the connection i am using to configure the EVM to EMDC without using isolation board as i am not giving external power 230V to the EVM.
below is the image i made connections to the EVM.
What else should I check to properly configure the EVM to EMDC?