Hello,
I connected the EVM to PC through RS-232 connection. using the steps mentioned in the below documentation.
https://www.ti.com/lit/an/slaa577g/slaa577g.pdf
i can only see the button is red.
I verified the connections even though it is showing red.
How to configure the EVM using the RS232 to the PC suggest me how to properly connect the Board to the PC.
the below is the schematic of the RS232 i am using to connect to the EVM board.
Thank you