This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969-SP: Using the MSP‑EXP430FR5969 eval board - need to program using BSL Interface

Part Number: MSP430FR5969-SP
Other Parts Discussed in Thread: MSP-FET

Hi,

I have the MSP‑EXP430FR5969 evaluation board along with a version of CCS. I am able to run a few of the SW examples provided. The eval board is connected via the USB interface to my PC.

It appears that the programming of the SW examples is done by SBW and I am wondering if there is a way to program this device using BSL?

I want to be able to program using BSL and then use the same interface as a UART interface once BSL programming in complete.

I also have the MSP-FET and the MSP-TS430RGZ84C devices.

Thanks!

 

**Attention** This is a public forum