Hello TI team,
at my company we are making other type of energymeter by using the TI's energymeter. But we have only few changes in the hardware. Because of that i have to make changes in the code.
If we are using the different type of current sensor which provides input value of 900 mV and 60 A for this energymeter then what changes i have to make in the source code can you tell me ? Also in which file? where?
As far as seen in the manual (Page 21), They have mentioned that voltage across current I1+ and current I1- must not exceed 930mV .But they havent mentioned anything about the current range . so can i use current sensor which gives input of 900mV and 60 A?? Do i have to make any changes in code because of this ?
Another question: In our energymeter we are not using the display. So i have removed the code content which contains display regarding code. Does it affect any other values ?
We are also removing the Aux vcc headers, DGND headers. and volatge monitor which is connected to pin 34 in the schematic of energymeter. Do i have to make changes in the code if we remove this components? or it will work without any problem?
Thank you very much.
Sincerely,
Abhi