Part Number: EVM430-FR6047
Other Parts Discussed in Thread: UNIFLASH
Hi
I am trying to measure the current consumption of the MSP430 processor and I am using the EVM430-FR6047.
I know there are jumpers that allow current measurement.
I connect the board to the sensors and to the computer.
1) Is the current measurement only for the MSP430?
Or the whole board?
2) When I connect to the board, connect to the GUI, the ADC is well, and perform water flow measurements, I reach a current consumption of 180u, which is very far from what I expect according to the datasheet.
The measurement is made by connecting a DVM between the two jumpers.
I would be happy to help on this matter.