Part Number: MSP430FR6043
Other Parts Discussed in Thread: MSP430FR6047, TDC7200
Hello,
I wish to implement a smart water-meter.
the requirements listed below :
- It must be possible to measure water flow accurately
20-320 liters/h - <5% error
320 - 5000 liters/h - <2% error - low power and battery powered device.
- lorawan, WalkBy, NB-IOT and Sigfox communication enabled.
Questions :
- Could you please suggest which absolute TOF measurement approach is better for this requirement (TDC Based Zero Crossing Approach / ADC Based Correlation Approach )? i am very confused on this.
- Can you suggest a good MCU for this project.
- Could you please suggest a good ultrasonic transducer for this requirement?
- Is MSP430FR6043 / MSP430FR6047 and ADC Based Correlation approach accurate as - TDC with "highly accurate timer such as TDC7200 with picosecond resolution is required. "
Thanks in advance