This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: C# help with which functions show which device is Connected and the Program status of the Board.

Part Number: MSP-GANG


I'm creating a C# application that I want to check if I'm Connected to a Board on one of the 8 spots for the MSP-GANG. In the GANG Programmer UI that is provided, in the Results section it Shows Connect and Program. I'm trying to figure out which function Can I call that will relay this information. I thought it might be the MSP_GetProgressStatus but I'm not receiving any data back. I could be doing something wrong just wanted to get some help.

**Attention** This is a public forum