Hey E2E Team,
i have a problem regarding the MTIF pulsgeneration. I tried to understand its function using Example msp430fr6043_mtif_02.c but i don't get it at all.
Firstly with the example of 8 pulses per 250ms, i tried to see after 10 seconds the number of pulse it should be 320 pulses, but i get 316 and i wonder why the 4 pulse are missing.
secondly i don't see any difference if i use PGFS_0, or PGFS_7, or other PGFS defined in msp430fr6043.h, so i don't undertand, which criteria i have look at in order to choose PGFS.
the third and last one, i don't really understand how got MTIFPGKVAL = 4, in order to have 8 pulses in 250ms. what should be my MTIFPGKVAL if i want for example to have 200 pulses per second assuming PGS is PGFS_7 and how did you get this MTIFPGKVAL?
thank you