Other Parts Discussed in Thread: MSP430F6779
Hi,
About the problem that i have been checking about the MCU get stuck (device does not start).
The MCU get stuck (the device not start) in the actual use field. But it cannot be reproduced in a laboratory.
This cannot use the debugger to debug where the code is stuck. (because the debugger reset the program counter)
Symptoms of the bug were just checked with the H/W pin
(device does not start).
DVCC: 3.419V, AUXVCC1: 3.328V
Vcore pin = 1.42 V (core level 0 AM)
Reset pin = 3.3 V
Now, i suspected cause from slow rising time and falling time as seen from old discuss in forum below.
https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/722493/msp430f6726-cause-and-remedy-to-make-the-mcu-immovable-state/2672286?tisearch=e2e-sitesearch&keymatch=delay%25252525252525252520BOR#2672286
[Power off → Rise speed at power on at around 1-2 V]
Power system A(MCU immovable state after Reset) : 2.13V/s(typ)
Power system B(MCU Normal state after Reset) : 2.68V/s(typ)
[Power off → Fall speed at power on at around 1-2 V]
Power system A(MCU immovable state after Reset) : 0.52V/s(typ)
Power system B(MCU Normal state after Reset) : 0.49V/s(typ)
So I have some questions below.
What is the rise time and fall time rate of the DVCC with the BOR circuit operating correctly (3 V/s)?
What happens when DVCC rise time and fall time are slower than 3 V/s (MCU stuck)?
Does the VDSYS have to consider the rise time and fall time rates for the BOR circuit to function properly?