Hi,
I am trying to connect MSP430FG4618 board to 'RS232 to RS485' converter for Modbus communication. Problem is that data sent from MSP430 UART, is not appearing at the RS485 side of 'RS232 to RS485 Converter', when observed on the DSO. Baud rate set is 9600, 18E
Following are more observations:
1. When Coverter is connected to RS232 of PC and Data sent from hyperterminal----> Data is received at the RS485 side of converter which can be observed on DSO.
2.. Data sent from MSP430 UART ----> Can be observed on the hyperterminal of the PC. [i.e serial comm of MSP430 is working]
3. When connected to PC, converter is port powered. No externer supply was required.
4. In case of MSP430 both approaches of connecting converter i.e Port Powered and External power supply +-12V were used. None of the approach worked.
Please suggest what might be going wrong.