Part Number: MSP430FR6047
Other Parts Discussed in Thread: EVM430-FR6047,
hello
Our company is producing a custom board based on EVM430-FR6047.
In the custom board, MSP430fr6047's P2.0: UCA0TXD, P2.1: UCA0RXD pins were configured as debug UART ports.
The debug UART part of the custom board is as follows.


And, to check degug UART operation, I programmed FW for TEST.
However, when only USBtoUART is connected to the custom board while all other cables, including the power source, are disconnected, the msp430fr6047 starts booting.
And, debugging is output from the USBtoUART port without power connection.

I'm inquiring because I don't understand why it boots by just connecting the UART even though the power is not connected.
The HW person in charge does not understand, so I would like to ask if this is normal or if the HW design is incorrect.
Additionally, if you have any advice or references regarding HW design, please ask.
The document referenced by HW was TIDRW71A-EVM.pdf.